Nominal_Current
| Index.Sub | |
| Data Type | Unsigned16 |
| Access | Read/Write |
| PDO Mappable | RX_PDO (1) |
| Unit |
milliamperes (mA) |
|
Range |
0 to (max drive current) |
| Default Value | 65535 |
| Store Supported | Yes |
| Description | This object defines the rated current (rms) of the motor. If value = 65535 no rated current is defined. |
|
Notes |
(1) available with firmware V03r02 or superior. |